Stepper Motors

A stepper motor is used as an output in electronic circuits. The motor is a brushless DC electric motor that divides a full rotation into a number of equal steps.

The motor’s position can then be made to move and hold at one of these steps without any position sensor for feedback as long as the motor is carefully sized to the application in respect to torque and speed.

Multiple coils are organised in phases (groups). By energising each phase in sequence the motor will rotate, one step at a time.

Why and when to use a Stepper Motor?

With a computer controlled stepping you can achieve very precise positioning and/or speed control.
•Steppers move in precise repeatable steps, they are perfect to use where precise positioning is needed such as 3D printers, CNC and camera platforms.


•Some disk drives use stepper motors to position the read/write head.


•Precise increments of movement also allow for excellent control of rotational speed for process automation and robotics.


•A Stepper motor has maximum torque at low speeds, so they are a good choice for applications where low speed with high precision is needed.



Stepper motor types
•Bipolar drivers use H bridge circuitry to reverse the current flow through the phases. By energising the phases with alternating the polarity all the coils can be put to work turning the motor.


•Permanent magnet motors use a permanent magnet in the rotor. They operate based on the principle that minimum reluctance occurs with minimum gap, meaning the rotor points are attracted towards the stator magnet poles.


•Unipolar drivers always energise the groups in the same way. The common lead will always be negative. They can be implemented with simple transistor circuitry.



Advantages of step motors
•Low cost


•High reliability


•High torque at low speed


•Full torque at standstill

...
Lees meer Lees minder

Filters

Uw huidige combinatie van filters heeft geen resultaten opgeleverd. Graag uw selectie aanpassen.