Vacuum Gauges

Vacuum Gauges are used to measure pressures lower than ambient atmospheric pressure, which is set as the zero points, in negative values for example -15 psig or -760 mmH equals total vacuum.


The inside of a tube which is bent into a circular arc (the so-called Bourdon tube) is connected to the vacuum system. Due to the effect of the external atmospheric pressure, the end of the tube bends more or less during the evacuation process.


Operating Temperature of Vacuum Gauge


It is the full-required range of ambient operating temperatures. Temperature and pressure in a system are directly related to each other. If the temperature of the closed operating environment increases, the pressure in the system will increase. In order to prevent equipment damage, it is important to know the extreme temperature ranges of the area.


The accuracy of Vacuum Gauge


It is the difference between the true value and the indication expressed as a percentage of the span. It includes the combined effects of method, observer, apparatus and environment.


What is Media?


Media is the term used to describe the material that surrounds the area of vacuum. Some vacuum gauges measure the pressures of liquids. Others measure the pressures of solids. Devices are also available that are rated for hazardous duty or for unlisted, specialized or proprietary materials.


Display type of Vacuum Gauge


  • Analogue - Analog meters are simple visual indicators using a dial

  • Digital meters - Digital meters are visual indicators with numerical valves

  • Cathode ray tube (CRT) - CRTs are commonly found in computer monitors

  • Liquid crystal display (LCD) - LCDs are semiconductor light sources using electrons which recombine with electron holes within the device and releasing energy in the form of photons

  • Multi-line video display - Video displays allow the user to watch and record live feeds of pressure changes in the system

Where is Vacuum Gauge used?


Vacuums are used in many industrial applications such as automotive, nautical, research and development, and manufacturing. They may be used to keep materials moving through the system or to keep the work area clean of pollutants. Gauges and instruments, such as sensors, are an important component to ensure the proper function and safety of the system and equipment.



Other typical applications include chemical and petroleum refineries, pharmaceutical, offshore drilling and production, paper mills, fertilizer.


...
Lees meer Lees minder

Filters

1 - 2 van 2 producten worden weergegeven
Resultaten per pagina
Omschrijving Prijs Best Accuracy Pressure Gauge Type Maximum Pressure Measurement Minimum Pressure Measurement Gauge Outside Diameter Connection Size Maximum Operating Temperature Minimum Operating Temperature Case Material Calibrated
RS-stocknr. 2509542831
FabrikantnummerGZ43-K-01
FabrikantSMC
€ 17,56
Each
Aantal stuks
- - - - - - - - - -
RS-stocknr. 2509542825
FabrikantnummerGZ33-K-01
FabrikantSMC
€ 13,20
Each
Aantal stuks
- - - - - - - - - -